VBUS.ICAP

Description

This parameter reports the instantaneous RMS current going through the internal electrolytic capacitors of the drive.


  • This parameter is not calculated at low bus voltages to avoid spurious bus capacitor overload faults.

Usage

To protect the internal electrolytic capacitors of the drive, if VBUS.ICAP goes above VBUS.ICAPLIMIT, a fault is thrown and the drive is disabled. Fault F2008: Bus capacitor overloaded.

General Information

Type Read Only
Units ARMS
Data Type Float

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

VBUS.ICAP

300ah

0ch

Signed32

-

1000:1

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

2503

1

2503 (0x9c7)

VBUS.ICAP

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

VBUS.ICAP

2503

Float

Read Only

-