VBUS.ICAPLIMIT
Description
This parameter reports the limit for RMS current going through the internal electrolytic capacitors of the drive.
Usage
To protect the internal electrolytic capacitors of the drive, if VBUS.ICAP goes above VBUS.ICAPLIMIT, a fault is thrown and the drive is disabled. Fault F2008: Bus capacitor overloaded.
General Information
|
Type |
Read Only |
|
Units |
ARMS |
|
Data Type |
Float |
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
VBUS.ICAPLIMIT |
300ah |
0dh |
Signed32 |
- |
1000:1 |
Read only |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
2504 |
1 |
2504 (0x9c8) |
VBUS.ICAPLIMIT |
Signed32 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
VBUS.ICAPLIMIT |
2504 |
Float |
Read Only |
- |