AXIS#.SAFE.FSOE.APPLPARAMLENGTH
Description
Indicates the size of the FSoE application parameters. If using WorkBench safety parameters, this is 0 and if using application parameters over FSoE it is 4 bytes.
Context
For complete FSoE information refer to the AKD2G EtherCAT Manual.
Versions
|
Action |
Version |
Notes |
|---|---|---|
|
Implemented |
02-01-02-000 |
|
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
0-65535 |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
No |
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.SAFE.FSOE.APPLPARAMLENGTH |
e901h |
08h |
Unsigned16 |
- |
- |
Read only |
No |
|
AXIS2.SAFE.FSOE.APPLPARAMLENGTH |
e911h |
08h |
Unsigned16 |
- |
- |
Read only |
No |