AXIS#.SAFE.FSOE.STATE

Description

This is the EtherCAT FSoE command word being sent to the drive from the FSoE master.

Value

Description

0x36

ProcessData – Process data is passed between FSoE master and slave.

0x2A

Reset – FSoE communication is in reset state.

0x4E

Session – FSoE session is being established between master and slave.

0x64

Connection – FSoE connection is being established between master and slave.

0x52

Parameter – Safe parameters are being downloaded to slave.

0x08

FailSafeData – Fail-safe values are being used (usually due to an error).

Context

For complete FSoE information refer to the AKD2G EtherCAT Manual.

Versions

Action

Version

Notes

Implemented

02-01-02-000

General Information

Type

Read Only

Units

N/A

Range

0x08, 0x2A, 0x36, 0x4E, 0x52, 0x64

Default Value

N/A

Data Type

Integer

Stored in Non-Volatile Memory

No

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFE.FSOE.STATE

e600h

01h

Unsigned8

-

-

Read only

No

AXIS2.SAFE.FSOE.STATE

e610h

01h

Unsigned8

-

-

Read only

No

AXIS1.SAFE.FSOE.STATE

e700h

01h

Unsigned8

-

-

Read only

No

AXIS2.SAFE.FSOE.STATE

e710h

01h

Unsigned8

-

-

Read only

No