AXIS#.SAFE.TEMPWARNING.ACTIVE
Description
Indicates whether the SMM temperature is in the expected range.
| Value | Description |
|---|---|
|
0 |
SMM temperature is not in the expected range |
|
1 |
SMM temperature is ok |
Versions
|
Action |
Version |
Notes |
|---|---|---|
|
Implemented |
2-00-00-000 |
Implemented in SMM revision v0.56 |
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
0, 1 |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
No |
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.SAFE.TEMPWARNING.ACTIVE |
2062h |
00h |
Unsigned8 |
- |
- |
Read only |
Yes |
|
AXIS2.SAFE.TEMPWARNING.ACTIVE |
2162h |
00h |
Unsigned8 |
- |
- |
Read only |
Yes |