AXIS#.SAFE.FUNCTIONGRAPH
This parameter returns the graph of the safety functions configured in the safety parameters.
The following format is used:
NODEID: Name(NODENAME); Type(NODETYPE); State(NODESTATE); FunctionSource(LIST_OF_FUNCTION_SOURCE); FaultReactionSource(LIST_OF_FAULT_REACTION); InputSource(LIST_OF_INPUTSOURCE); FSoESource(LIST_OF_FSOE_SOURCE); Properties(LIST_OF_PROPERTIES)
- NODEID: node unique ID, built as follows:
- Safe functions: SOS, SS1_1, SLS_3, ...
- Safe inputs: SIN1_SOS, SINDUAL2_SS1_2, ...
- FSoE: FSOE_SOS, FSOE_SS1_1, ...
- I/O Error: IOError
- NODENAME: function name to display (eg FSoE, SIN1, SS1_1, ...) [displayed in the block]
- NODETYPE: node type – SIN, SINDUAL, FSOE, FUNCTION, ERROR [type of graphical block]
- NODESTATE can be: [colorization of the block]
- For FUNCTION: “Idle”, “ProcessComplete”, “Active”, “Faulted”
- For SIN, SINDUAL or FSoE: “On”, “Off”
- For ERROR: “Normal”, “Error”
- LIST_OF_FUNCTION_SOURCE, LIST_OF_FAULT_REACTION, LIST_OF_INPUTSOURCE and LIST_OF_FSOE_SOURCE are a list of NODEIDs separated by a comma
- LIST_OF_PROPERTIES: string list to display separated by commas
Versions
| Action | Version | Notes |
|---|---|---|
|
Implemented |
Next release |
Implemented in SMM revision v0.54 |
General Information
|
Type |
Info |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
Stored in Non-Volatile Memory |
N/A |