AXIS#.SAFEPARAM.SOS.FSOE

Description

Indicates if the Safe Operating Stop (SOS) function can be activated through FSoE. This parameter can only set to “Used” when FSoE is activated (SAFEPARAM.SAFEFIELDBUS.ACTIVATION is set to 1 – “Activated”).

Value Description

0

Not used

1

Used

 

Context

For complete SOS information refer to SOS (Safe Operating Stop).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.54

General Information

Type

Read/Write

Units

N/A

Range

0, 1

Default Value

0 (Not used)

Data Type

Integer

Stored in Non Volatile Memory

No

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SOS.FSOE

315bh

03h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SOS.FSOE

325bh

03h

Unsigned8

-

-

Read/Write

No