AXIS#.SAFEPARAM.UNIT.ACCINENC

Description

Indicates the acceleration increment in encoder units.

 

The safe system uses the following formula:

With:

  • accInEncUnit is AXIS#.SAFEPARAM.UNIT.ACCINENC
  • accInUserUnit is AXIS#.SAFEPARAM.UNIT.ACCINUSER
  • resInNbInc: the encoder resolution in counts
  • resInEncUnit: resolution in encoder units

Example

  • accInEncUnit is AXIS#.SAFEPARAM.UNIT.ACCINENC
  • accInUserUnit is AXIS#.SAFEPARAM.UNIT.ACCINUSER
Acceleration: accInUserUnit[accUserUnit] = accInEncUnit[encUnit/s^2] 
Acceleration∶ 60[rpm/s]=1[rev/s^2]
Acceleration∶ 1[mm/s^2]=1000000 [nm/s^2]

Context

For details refer to Parameterization of User Units.

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

User defined

Range

N/A

Default Value

1

Data Type

Integer

Stored in Non-Volatile Memory

No

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.UNIT.ACCINENC

3151h

0ah

Unsigned32

-

-

Read/Write

No

AXIS2.SAFEPARAM.UNIT.ACCINENC

3251h

0ah

Unsigned32

-

-

Read/Write

No