SAFE.CHANGEPASSWORD
Description
Change or create the password used for safety parameters operation. The master password remains unchanged and valid. The password must be at least 8 characters long but not more than 25 characters. This password cannot be retrieved if lost but the master password can be used to reset it.
|
The master password is SafeMotionMonitorXXX where XXX are the last 3 digits of the drive serial number. |
Usage
SAFE.CHANGEPASSWORD <new_password> <confirmation_password>
All parameters are mandatory. The drive will return an error if:
- Not enough parameters are provided .
- Too much parameters are provided .
- At least one of the parameter is out of range.
- The confirmation password is not valid (error returned by the SMM)
|
The password strings cannot contain any spaces. |
<new_password>: String of 8 bytes min and 25 bytes max
<confirmation_password>: String of 8 bytes min and 25 bytes max
Versions
|
Action |
Version |
Notes |
|---|---|---|
|
Implemented |
02-00-00-000 |
Implemented in SMM revision v0.32 |
General Information
|
Type |
Command |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
Stored in Non-Volatile Memory |
No |