SAFEPARAM.IOFAILUREACKSOURCE
Description
Indicates which safe input, if any, is configured as the I/O Failure acknowledge source. This parameter is configured using FSoE or WorkBench . When configured, it allows clearing of an I/O Failure warning (W9011) using the configured safety input.
Versions
|
Action |
Version |
Notes |
|---|---|---|
|
Implemented |
02-01-02-000 |
|
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0...4 |
|
Default Value |
0 (No safe input) |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
No |
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
SAFEPARAM.IOFAILUREACKSOURCE |
3100h |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |