Controller Rotary Switch
The rotary switch on a Kollmorgen controller is set from a 0 to 9 position.
|
Switch Position |
Description |
|---|---|
|
Position 0 |
|
|
Position 1 |
Either:
|
|
Position 2-9 |
|
-
-
If a DHCP server is not present, the drive assumes an Automatic Private IP Address of the form 169.254.x.x.
-
-
The AKD PDMM and PCMM do not set (or show) an IP address without an attached network cable.
On the PCMM2G, if a network cable is not attached or no IP address is assigned, the controller shows an IP address of 0.0.0.0.