Motion State Machine
The Motion State Machine is driven by the IEC 61131-3 application with the help of dedicated function blocks.
See (➜ # 1, Motion / Common - Motion) for more information about the functions that prepare the physical motion part.
Figure 1: Motion State Machine
Each arrow represents a transition from one state to another.