Add CoE Commands

This command is used to construct a new Init Command by supplying Index, Subindex, Value, Comment, Transition, and Direction attributes.

  • The dialog lists the device's object dictionary.
  • The objects are filtered based on the selected in the Direction drop-down.
    • Example: If Write is selected, the Read-only objects are not shown. (Figure 1)

Figure 1: Direction drop-down selection: Write


    • The Index field accepts four characters at most.
    • The Subindex has a range of 0 - 255.
    • When setting the Direction you may select Read or Write.
    • Selecting an item in the CoE Object-Dictionary auto-populates the Index and Subindex entries.

The Next button is available once the Index and Subindex fields have values.