Backup and Restore from the Web server

The Backup and Restore functions are used to replicate a Kollmorgen controller.

The controller data is replicated on the PCMM2G USB flash drive.

All Controllers

The elements that are backed up or restored for all controllers are:

  • Controller firmware.
  • Network configuration.
  • PLC Application.
  • Retain Variables.
  • Shared Directory settings.
  • User data files.
  • Web server and SSH user accounts configuration.

PCMM2G Backup / Restore Only

Backup

  • Date/Time - Network Time Protocol (NTP) and Set Time Zone settings.
  • SSH Connection Enable/Disable configuration.
  • AKD / AKD2G / Kollmorgen Essentials Drive firmware packages and their respective drive parameters.
  • EtherCAT network topology.

Restore

  • The drive's data and firmware are copied from the USB flash drive to the controller flash when the Restore Controller function is selected.
  • The Restore EtherCAT Devices function should be selected for restoring the data and the firmware of any replaced Kollmorgen AKD Series Servo Drives.

    • A PCMM2G backup created from any PCMM2G axis model can be restored on a different axis model.
    • The restored KAS project does not run if the physical axes need for the project is more than the restored model can support.

The Backup and Restore processes:

  • Cannot be performed while an application is running.
  • Takes several minutes to complete.
    • Do not power off the controller once started.
  • The controller is rebooted after a Restore.

  • AKD PDMM or PCMM do not allow restoring the controller from the PCMM2G backup.
    PCMM2G does not allow restoring the controller from the AKD PDMM or PCMM backups.

The AKD PDMM and PCMM are available with different CPU variants (800MHz, 1.2GHz single core, and 1.2GHz dual core).

  • The AKD PDMM and PCMM models have the same functionality but, because of CPU speed differences, an application designed for the 1.2GHz model may not execute as expected on the 800MHz model.
    • An application designed for a single core CPU model may not execute as expected on the dual core model.
  • The Restore:
    • Does not allow a higher speed model to be replaced with a lower speed model.
    • Does allow a lower speed model to be replaced with a higher speed model if the Backup contains the model-specific Runtime firmware file.

Backup File Source

PCMM2G Restore

PCMM2G Backup

Yes

800MHz Backup

No

1.2GHz Single Core Backup

No

1.2GHz Dual Core Backup

No