USB Flash Drive tab
-
-
This tab is only visible for PCMM2G controllers.
Figure 1: USB Flash Drive tab
This tab is used to format the USB flash drive as FAT32.
-
- PCMM2G supports only one USB flash drive.
If a USB hub is used to expand the USB ports on the PCMM2G, use only a single USB flash drive in the hub.
-
- All data is erased from the USB flash drive.
The Format function cannot be performed while an application is running.