Plug a Probe from the Pipe Network

A probe (variable) can be directly plugged or mapped to the Oscilloscope from the Pipe Network.

Procedure

  1. Right-click on a Pipe Block.
  2. In the menu, click the Map to Oscilloscope channel …. (Figure 1)
  3. Plug a Probe from the Pipe Network

    Figure 1: Map to Oscilloscope channel … menu option

    The Map to Oscilloscope channel … dialog box opens. (Figure 2)

    Figure 2: Map to Oscilloscope channel … dialog box

  4. Define the probe parameters.

Field

Description

Channel

Channel's number where the variable has to be plugged

Data

Desired variable information to show (the list depends on the type of Pipe Block.

Derivation Order

  • Performs a derivation of the measurement of the selected variable.
  • If this value is different from 0 (zero), the derived value of the selected order is shown on the selected channel.

Derivation Period

  • Specifies the modulo period for a periodic variable to remove spikes in the display of derivative orders greater than zero.
  • The value entered should either be 0.0 (No Modulo) or the Modulo Period (e.g., 360.0).

Name

Variable's name.

Type

Variable's type.

 


  • The Map to Oscilloscope channel … menu option is disabled if the KAS-IDE is not connected to the controller or if the project is not running.

    This menu option is disabled when the Trace Times Channel Group is selected in the Oscilloscope Control Panel.