Help menu

Menu Option

Description

Documentation

Opens the help system.

Help Preference

As stated in Is the Help System Online or Offline?, there is more than one type of help system with different advantages.

  • Click the Use Online Documentation option to open the online help.
    • This is the default selection.
  • Click the Use Offline Documentation option to open the locally installed help (if available).

Kollmorgen Support Network (KSN)

Opens a web browser to the Kollmorgen Support Network, a community support site.

About