ACTION#.SOURCEID

Description

Some action sources require a specific source ID number. For example, if your action source is a Digital Input, then a source ID of 1 would correspond to Digital Input 1.

The range of the source ID will depend on the value of the corresponding source. If the source is modified, the range and units of the source ID may change, and the source ID value will default to the first valid value.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Depends on ACTION#.SOURCE

Range

Depends on ACTION#.SOURCE

Default Value

0

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

ACTION1.SOURCEID

3905h

01h

Unsigned8

-

-

Read/Write

No

ACTION2.SOURCEID

3905h

02h

Unsigned8

-

-

Read/Write

No

ACTION3.SOURCEID

3905h

03h

Unsigned8

-

-

Read/Write

No

ACTION4.SOURCEID

3905h

04h

Unsigned8

-

-

Read/Write

No

ACTION5.SOURCEID

3905h

05h

Unsigned8

-

-

Read/Write

No

ACTION6.SOURCEID

3905h

06h

Unsigned8

-

-

Read/Write

No

ACTION7.SOURCEID

3905h

07h

Unsigned8

-

-

Read/Write

No

ACTION8.SOURCEID

3905h

08h

Unsigned8

-

-

Read/Write

No

ACTION9.SOURCEID

3905h

09h

Unsigned8

-

-

Read/Write

No

ACTION10.SOURCEID

3905h

0ah

Unsigned8

-

-

Read/Write

No

ACTION11.SOURCEID

3905h

0bh

Unsigned8

-

-

Read/Write

No

ACTION12.SOURCEID

3905h

0ch

Unsigned8

-

-

Read/Write

No

ACTION13.SOURCEID

3905h

0dh

Unsigned8

-

-

Read/Write

No

ACTION14.SOURCEID

3905h

0eh

Unsigned8

-

-

Read/Write

No

ACTION15.SOURCEID

3905h

0fh

Unsigned8

-

-

Read/Write

No

ACTION16.SOURCEID

3905h

10h

Unsigned8

-

-

Read/Write

No

ACTION17.SOURCEID

3905h

11h

Unsigned8

-

-

Read/Write

No

ACTION18.SOURCEID

3905h

12h

Unsigned8

-

-

Read/Write

No

ACTION19.SOURCEID

3905h

13h

Unsigned8

-

-

Read/Write

No

ACTION20.SOURCEID

3905h

14h

Unsigned8

-

-

Read/Write

No

ACTION21.SOURCEID

3905h

15h

Unsigned8

-

-

Read/Write

No

ACTION22.SOURCEID

3905h

16h

Unsigned8

-

-

Read/Write

No

ACTION23.SOURCEID

3905h

17h

Unsigned8

-

-

Read/Write

No

ACTION24.SOURCEID

3905h

18h

Unsigned8

-

-

Read/Write

No

ACTION25.SOURCEID

3905h

19h

Unsigned8

-

-

Read/Write

No

ACTION26.SOURCEID

3905h

1ah

Unsigned8

-

-

Read/Write

No

ACTION27.SOURCEID

3905h

1bh

Unsigned8

-

-

Read/Write

No

ACTION28.SOURCEID

3905h

1ch

Unsigned8

-

-

Read/Write

No

ACTION29.SOURCEID

3905h

1dh

Unsigned8

-

-

Read/Write

No

ACTION30.SOURCEID

3905h

1eh

Unsigned8

-

-

Read/Write

No

ACTION31.SOURCEID

3905h

1fh

Unsigned8

-

-

Read/Write

No

ACTION32.SOURCEID

3905h

20h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

40600

1

40600 (0x9e98)

ACTION1.SOURCEID

Unsigned8

Read/Write

Yes

40601

1

40601 (0x9e99)

ACTION2.SOURCEID

Unsigned8

Read/Write

Yes

40602

1

40602 (0x9e9a)

ACTION3.SOURCEID

Unsigned8

Read/Write

Yes

40603

1

40603 (0x9e9b)

ACTION4.SOURCEID

Unsigned8

Read/Write

Yes

40604

1

40604 (0x9e9c)

ACTION5.SOURCEID

Unsigned8

Read/Write

Yes

40605

1

40605 (0x9e9d)

ACTION6.SOURCEID

Unsigned8

Read/Write

Yes

40606

1

40606 (0x9e9e)

ACTION7.SOURCEID

Unsigned8

Read/Write

Yes

40607

1

40607 (0x9e9f)

ACTION8.SOURCEID

Unsigned8

Read/Write

Yes

40608

1

40608 (0x9ea0)

ACTION9.SOURCEID

Unsigned8

Read/Write

Yes

40609

1

40609 (0x9ea1)

ACTION10.SOURCEID

Unsigned8

Read/Write

Yes

40610

1

40610 (0x9ea2)

ACTION11.SOURCEID

Unsigned8

Read/Write

Yes

40611

1

40611 (0x9ea3)

ACTION12.SOURCEID

Unsigned8

Read/Write

Yes

40612

1

40612 (0x9ea4)

ACTION13.SOURCEID

Unsigned8

Read/Write

Yes

40613

1

40613 (0x9ea5)

ACTION14.SOURCEID

Unsigned8

Read/Write

Yes

40614

1

40614 (0x9ea6)

ACTION15.SOURCEID

Unsigned8

Read/Write

Yes

40615

1

40615 (0x9ea7)

ACTION16.SOURCEID

Unsigned8

Read/Write

Yes

40616

1

40616 (0x9ea8)

ACTION17.SOURCEID

Unsigned8

Read/Write

Yes

40617

1

40617 (0x9ea9)

ACTION18.SOURCEID

Unsigned8

Read/Write

Yes

40618

1

40618 (0x9eaa)

ACTION19.SOURCEID

Unsigned8

Read/Write

Yes

40619

1

40619 (0x9eab)

ACTION20.SOURCEID

Unsigned8

Read/Write

Yes

40620

1

40620 (0x9eac)

ACTION21.SOURCEID

Unsigned8

Read/Write

Yes

40621

1

40621 (0x9ead)

ACTION22.SOURCEID

Unsigned8

Read/Write

Yes

40622

1

40622 (0x9eae)

ACTION23.SOURCEID

Unsigned8

Read/Write

Yes

40623

1

40623 (0x9eaf)

ACTION24.SOURCEID

Unsigned8

Read/Write

Yes

40624

1

40624 (0x9eb0)

ACTION25.SOURCEID

Unsigned8

Read/Write

Yes

40625

1

40625 (0x9eb1)

ACTION26.SOURCEID

Unsigned8

Read/Write

Yes

40626

1

40626 (0x9eb2)

ACTION27.SOURCEID

Unsigned8

Read/Write

Yes

40627

1

40627 (0x9eb3)

ACTION28.SOURCEID

Unsigned8

Read/Write

Yes

40628

1

40628 (0x9eb4)

ACTION29.SOURCEID

Unsigned8

Read/Write

Yes

40629

1

40629 (0x9eb5)

ACTION30.SOURCEID

Unsigned8

Read/Write

Yes

40630

1

40630 (0x9eb6)

ACTION31.SOURCEID

Unsigned8

Read/Write

Yes

40631

1

40631 (0x9eb7)

ACTION32.SOURCEID

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

ACTION1.SOURCEID

40600

Unsigned8

Read/Write

-

ACTION2.SOURCEID

40601

Unsigned8

Read/Write

-

ACTION3.SOURCEID

40602

Unsigned8

Read/Write

-

ACTION4.SOURCEID

40603

Unsigned8

Read/Write

-

ACTION5.SOURCEID

40604

Unsigned8

Read/Write

-

ACTION6.SOURCEID

40605

Unsigned8

Read/Write

-

ACTION7.SOURCEID

40606

Unsigned8

Read/Write

-

ACTION8.SOURCEID

40607

Unsigned8

Read/Write

-

ACTION9.SOURCEID

40608

Unsigned8

Read/Write

-

ACTION10.SOURCEID

40609

Unsigned8

Read/Write

-

ACTION11.SOURCEID

40610

Unsigned8

Read/Write

-

ACTION12.SOURCEID

40611

Unsigned8

Read/Write

-

ACTION13.SOURCEID

40612

Unsigned8

Read/Write

-

ACTION14.SOURCEID

40613

Unsigned8

Read/Write

-

ACTION15.SOURCEID

40614

Unsigned8

Read/Write

-

ACTION16.SOURCEID

40615

Unsigned8

Read/Write

-

ACTION17.SOURCEID

40616

Unsigned8

Read/Write

-

ACTION18.SOURCEID

40617

Unsigned8

Read/Write

-

ACTION19.SOURCEID

40618

Unsigned8

Read/Write

-

ACTION20.SOURCEID

40619

Unsigned8

Read/Write

-

ACTION21.SOURCEID

40620

Unsigned8

Read/Write

-

ACTION22.SOURCEID

40621

Unsigned8

Read/Write

-

ACTION23.SOURCEID

40622

Unsigned8

Read/Write

-

ACTION24.SOURCEID

40623

Unsigned8

Read/Write

-

ACTION25.SOURCEID

40624

Unsigned8

Read/Write

-

ACTION26.SOURCEID

40625

Unsigned8

Read/Write

-

ACTION27.SOURCEID

40626

Unsigned8

Read/Write

-

ACTION28.SOURCEID

40627

Unsigned8

Read/Write

-

ACTION29.SOURCEID

40628

Unsigned8

Read/Write

-

ACTION30.SOURCEID

40629

Unsigned8

Read/Write

-

ACTION31.SOURCEID

40630

Unsigned8

Read/Write

-

ACTION32.SOURCEID

40631

Unsigned8

Read/Write

-