AXIS#.IL.KVFF

Description

This parameter sets the gain for the velocity loop feedforward. It is used when you want to add a pure torque component scaled by the velocity command.

Resulting Torque Feedforward = AXIS#.TRAJ.VCMD * AXIS#.IL.KVFF

This parameter is only used in velocity and position mode (AXIS#.OPMODE = 1 and 2).

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

mArms / (rad/s)

Range

0 to 1,000,000

Default Value

0

Data Type

Float

See Also

AXIS#.IL.FF

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.IL.KVFF

500ah

0eh

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5812

1

5812 (0x16b4)

AXIS1.IL.KVFF

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.IL.KVFF

5812

Float

Read/Write

-