AXIS#.TUNING.QUICKTUNE.START
Description
AXIS#.TUNING.QUICKTUNE.START triggers the execution of the QuickTune procedure and is responsible for taking an inertia measurement of the load and then calculating an ideal target bandwidth. The axis must be enabled for this procedure to run. After the procedure has finished successfully AXIS#.TUNING.BANDWIDTH will be set to either the AXIS#.TUNING.TARGETBANDWIDTH or AXIS#.TUNING.USERBANDWIDTH value and the drive is tuned accordingly.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-12-02-000 |
- |
General Information
| Type | Command |
| Units | N/A |
| Range | N/A |
| Default Value | N/A |
| Data Type | N/A |
| See Also | AXIS#.TUNING.BANDWIDTH |
| Stored in Non-Volatile Memory | No |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.TUNING.QUICKTUNE.START |
5021h |
05h |
Unsigned32 |
- |
- |
Write only |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
5042 |
1 |
5042 (0x13b2) |
AXIS1.TUNING.QUICKTUNE.START |
Unsigned8 |
Read/Write |
No |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS1.TUNING.QUICKTUNE.START |
5042 |
Unsigned8 |
Read/Write |
- |