PWM#.PERIOD
Description
Sets the period length of the PWM signal, that can be output on a digital IO with DIO#.SOURCE 6.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-11-03-000 |
General Information
| Type | Read/Write |
| Units | Microseconds |
| Range | 1 to 500 |
| Default Value | 1 |
| Data Type | Integer |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
PWM1.PERIOD |
38f0h |
01h |
Unsigned16 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
42105 |
1 |
42105 (0xa479) |
PWM1.PERIOD |
Unsigned16 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
PWM1.PERIOD |
42105 |
Unsigned16 |
Read/Write |
- |