REC.TRIGSLOPE
Description
REC.TRIGSLOPE sets the recorder trigger slope. This parameter is not used when REC.TRIGTYPE is 0 or 1.
| Value | Description |
|---|---|
| 0 | Negative |
| 1 | Positive |
Example
Code
Trigger the capture on a positive rate of change.
-->REC.TRIGSLOPE 1
Context
For more information see Scope.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
1 |
|
Data Type |
Integer |
|
See Also |
|
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
2309 |
1 |
2309 (0x905) |
REC.TRIGSLOPE |
Unsigned8 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
REC.TRIGSLOPE |
2309 |
Unsigned8 |
Read/Write |
- |