MOTOR.TEMP
Description
This parameter returns the motor temperature, which is represented as the resistance of the motor's PTC or NTC.
General Information
|
Type |
R/O Parameter |
|
Units |
Ω |
|
Range |
0 to 232 Ω |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Start Version |
M_01-00-00-000 |
| Variant | Supported |
|---|---|
| MKD EtherCAT | Yes |
| AKD-N | Yes |
| MKD-N | Yes |
| MKD-C | No |
| Index/Subindex | Object Start Version |
|---|---|
|
3612h/0 |
M_01-00-00-000 |
Related Topics