VBUS.VALUE
Description
VBUS.VALUE reads the DC bus voltage.
General Information
|
Type |
R/O Parameter |
|
Units |
VDC |
|
Range |
0 to 900VDC |
|
Default Value |
N/A |
|
Data Type |
Float |
|
See Also |
N/A |
|
Start Version |
M_01-00-00-000 |
| Variant | Supported |
|---|---|
| MKD EtherCAT | Yes |
| AKD-N | Yes |
| MKD-N | Yes |
| MKD-C | Yes |
| Index/Subindex | Object Start Version |
|---|---|
| 361Ah/0 | M_01-00-00-000 |
Related Topics
1 Regeneration