AXIS#.TUNING.INERTIA.MISMATCHMAX

Description

AXIS#.TUNING.INERTIA.MISMATCHMAX defines the maximum inertia mismatch ratio for the Inertia Measurement algorithm.

If the Inertia Measurement algorithm calculates an inertia that exceeds this maximum value then the inertia will be limited to the MISMATCHMAX multiplied by AXIS#.MOTOR.INERTIA .

If the Inertia Measurement algorithm is limited by AXIS#.TUNING.INERTIA.MISMATCHMAX, its state will indicate it completed successfully but was clamped.

Versions

Action Version Notes
Implemented 02-13-01-000 

-

General Information

Type Read / Write
Units N/A
Range 0.0 to 1000.0
Default Value 500.0
Data Type Double
See Also

AXIS#.TUNING.INERTIA.MEASURE

Stored in Non-Volatile Memory No

Variants Supported

All variants are supported.