AXIS#.VL.KP

Description

AXIS#.VL.KP sets the proportional gain of the velocity loop.

The idealized velocity loop bandwidth in Hz is:

Rotary motor:

Bandwidth (Hz) = AXIS#.VL.KP *Kt/ (2π *Jm)

Where:

Kt= motor torque constant, in units of Nm/Arms

Jm = motor inertia, in units of kg*m²

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

A/(rad/sec)

Range

0 to 2,147,483.008

Default Value

0

Data Type

Float

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.VL.KP

5011h

01h

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6029

1

6029 (0x178d)

AXIS1.VL.KP

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.VL.KP

6029

Float

Read/Write

-