AXIS#.DBILIMIT

Description

This parameter sets the maximum amplitude of the current for dynamic braking. AXIS#.DBILIMIT can only be set manually when AXIS#.MOTOR.DISAUTOSET index (28) is set to 1. Setting AXIS#.MOTOR.AUTOSET to 0 does not make AXIS#.DBILIMIT writeable.


  • If the motor or drive current is in foldback before entering dynamic brake mode, the actual current limit might be less than AXIS#.DBILIMIT when dynamic braking starts. The current will be limited to the minimum of AXIS#.DBILIMIT and AXIS#.IL.IFOLD . Once the foldback current recovers, AXIS#.DBILIMIT will be the enforced current limit.

Example

Setting AXIS#.DBILIMIT to 2 limits the dynamic brake current to 2 Arms.

Versions

Action Version Notes
Implemented 02-00-00-000
Bug fix 02-08-00-000 The bug caused AXIS#.DBILIMIT to be reset to its default value under some conditions. The fix involved making the parameter read only by default and calculated from motor parameters.

General Information

Type

Read/Write

Units

Arms

Range

0 to minimum of drive peak current (IPEAK) and motor peak current (AXIS#.MOTOR.IPEAK ).

Default Value

Drive continuous current (ICONT)

Data Type

Float

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.DBILIMIT

5000h

07h

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5005

1

5005 (0x138d)

AXIS1.DBILIMIT

Unsigned32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.DBILIMIT

5005

Float

Read Only

-