DIO#.SOURCEID

Description

DIO#.SOURCEID sets the digital I/O source ID, for sources that require an ID.

Examples

Usage

DIO#.SOURCEID can be used to select the compare channel whenDIO#.SOURCE = 4 (Compare).

Code

The following commands set the source of digital IO 1 to compare channel 1, and digital IO 2 to compare channel 2.

--> DIO1.SOURCE 4
--> DIO1.SOURCEID 1
--> DIO2.SOURCE 4
--> DIO2.SOURCEID 2

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000  
Added Compare source 02-06-00-000  

General Information

Type Read/Write
Units N/A
Range 1 to 2
Default Value 0
Data Type Integer
See Also  

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

DIO1.SOURCEID

368ah

06h

Unsigned8

-

-

Read/Write

No

DIO2.SOURCEID

368bh

06h

Unsigned8

-

-

Read/Write

No

DIO3.SOURCEID

368ch

06h

Unsigned8

-

-

Read/Write

No

DIO4.SOURCEID

368dh

06h

Unsigned8

-

-

Read/Write

No

DIO5.SOURCEID

368eh

06h

Unsigned8

-

-

Read/Write

No

DIO6.SOURCEID

368fh

06h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

22300

1

22300 (0x571c)

DIO1.SOURCEID

Unsigned8

Read/Write

Yes

22301

1

22301 (0x571d)

DIO2.SOURCEID

Unsigned8

Read/Write

Yes

22302

1

22302 (0x571e)

DIO3.SOURCEID

Unsigned8

Read/Write

Yes

22303

1

22303 (0x571f)

DIO4.SOURCEID

Unsigned8

Read/Write

Yes

22304

1

22304 (0x5720)

DIO5.SOURCEID

Unsigned8

Read/Write

Yes

22305

1

22305 (0x5721)

DIO6.SOURCEID

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

DIO1.SOURCEID

22300

Unsigned8

Read/Write

-

DIO2.SOURCEID

22301

Unsigned8

Read/Write

-

DIO3.SOURCEID

22302

Unsigned8

Read/Write

-

DIO4.SOURCEID

22303

Unsigned8

Read/Write

-

DIO5.SOURCEID

22304

Unsigned8

Read/Write

-

DIO6.SOURCEID

22305

Unsigned8

Read/Write

-