FB#.TRACKINGCAL

Description

This parameter turns the tracking calibration algorithm for 1 Vp-p analog sine-cosine feedback or resolver on or off. When enabled and the axis is moving, the interface nulls any offset, corrects gain mismatches between the two channels, and corrects the two channels to be exactly 90 degrees apart. This process automatically turns on above the set threshold of eitherFB#.CALTHRESHSINCOS (analog sine encoders) or FB#.CALTHRESHRES (relsover). When going below the threshold, the offset, gain, and quadrature adjustment values are sampled and held.

Use FB#.CALTHRESHSINCOS for 1 Vp-p analog sine-cosine feedback and FB#.CALTHRESHRES for resolver. This process makes the motion smoother while moving with less unintended acoustic noise. However, because the adjustments will slightly change move-to-move, the repeatability of position holds is slightly degraded.

1 = Tracking calibration is on.

0 = Tracking calibration is off.

Context

Only used for feedbacks with analog sine signals such as Sin/Cos, EnDat Analog, Resolver, etc. See Feedback # View.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

See Also

N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

FB1.TRACKINGCAL

3500h

10h

Unsigned8

-

-

Read/Write

No

FB2.TRACKINGCAL

3501h

10h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

30180

1

30180 (0x75e4)

FB1.TRACKINGCAL

Unsigned8

Read/Write

Yes

30181

1

30181 (0x75e5)

FB2.TRACKINGCAL

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.TRACKINGCAL

30180

Unsigned8

Read/Write

-

FB2.TRACKINGCAL

30181

Unsigned8

Read/Write

-