Automatic Tuning

The Automatic tuner uses default guidelines to determine tuning parameters that comply with the stability requirements.

Automatic Tuning Interface

  1. Top Ribbon

  2. Automatic Tuning Pane

  3. Measurement Pane

  4. Post-Processing

  5. Tuning Results Pane

Top Ribbon

Parameter Description  

Mode

Sets the tuning method.

New

Start Autotune initiates the automatic tuning process.

Settings

Populates the Settings Pane with Basic or Advanced parameters available. The Basic setting limits the Measurement Type to Plant and Closed Loop, and limits the Settings to only # FFT Points. The Advanced setting adds Current Loop and Custom to the Measurement Type options, as well as additional FFT values to the Settings options.

Default Settings: Resets all the editable parameters back to their default values.

Drive Tuning

Default Tuning: Resets the tuning parameters to the drive defaults at 75 Hz bandwidth.

Share

Export CSV files of the tuning data and parameters.

Status

Shows the stability rating of the Autotune results.

Automatic Tuning Pane

Parameter

Explanation

Desired Bandwidth

Defines the fixed bandwidth of 100 Hz that the Autotuner tries to achieve. This parameter is not user editable.

Gain & Phase Margin

Specifies how “hot” to tune the system. As the user lowers the margins, the Autotuner will achieve higher gains and higher system bandwidth, but stability will decrease.


  • Often the increase in bandwidth is not worth the loss in stability.
  •  

Tune Acceleration FF

When checked, the Autotuner will calculate the acceleration feed forward for the system, and write it to the drive.

Enable Stability Motion

If checked, a short move will be performed at the end of Automatic tuning and a stability algorithm verify that the control loop is stable.

Measurement Pane

Parameter Options Description

Excitation Type

1 - PRB

Uses a pseudo random binary signal to excite the system. The signal is either positive (+) or negative (–) current or velocity amplitude (depending the injection point).

2 - Sine

Requires the start frequency, end frequency, and frequency step size be specified. The sine sweep takes significantly longer than a noise or PRB measurement but is often cleaner. Choose the step size carefully: a step size that is too large may miss important resonances, and a step size that is too small increases measurement time.

3 - Noise

Uses a pseudo random noise signal to excite the system. The signal varies between positive (+)/negative (-) current or velocity amplitude (depending on injection point).

Excitation Configuration Mode

0 - User Defined

User sets the Excitation Current.

1 - Friction Test

The tuner will begin with a friction test to determine how much excitation is needed to acquire accurate data.The minimum current required to command continuous motion becomes the excitation current.

Excitation Current

Current appliedy to excite the system

User defined, or determined from Friction Test. See Excitation Current for more information.

# FFT Points

Default value: 4096

From 1024 to 32768

FFT Resolution is used to generate a Bode plot from measured data.

# Points to Record

Determined by the # FFT

Points chosen by default

Total number of sampled data points.

Sampling Frequency

Default 8000,

Range: 500, 1000, 2000, 4000, and 8000

Rate at which the points are sampled.

FFT Overlap

Percentage

Percentage of overlap of time blocks

Max Velocity

Sets AKD2G:AXIS#.VL.THRESH to a maximum velocity for the excitation tests. If the excitation causes the motor to exceed this value, a Motor Overspeed fault is thrown.

Post-Processing

Raw Measurement Smoothing smooths noisy or low-resolution data. See Post Processing Smoothing %.

Tuning Results Pane

The Results pane provides the general and detailed tuning results, along with the tuning parameters values used. The results can be copied and pasted in any text editor.

View the resultant Bode and Nichols plots by clicking the link in the Results pane, or switching to Manual mode.

Automatic Tuning Procedure

The Autotuner uses default guidelines to determine tuning parameters that comply with stability requirements.

The Autotuner will tune the system using the following settings:

The Autotuner will tune the system using the following settings:

  • Position Loop Proportional (PL.KP)

  • Velocity Loop Proportional (VL.KP)

  • Anti Resonance Filter 1 Set to Lead Lag (AR1)

  • Anti Resonance Filter 3 (AR3) & 4 (AR4) set to Lowpass

    • These are set to reduce audible noise.


  • These settings cannot be changed and will always be tuned.

 

To Get Started:

  1. Put the drive in Velocity or Position mode depending on how the axis will be operated.

  2. Adjust any user-definable as desired.

  3. Start Autotune.

Results

Once the Autotuner finishes, the Status and Results pane will appear. The Status is a visual representation of the Stability Rating shown in the Results pane.

The Results pane provides the general and detailed tuning results, along with the values of the tuning parameters used. The results can be copied and pasted in any text editor.

View the resultant Bode and Nichols plots by clicking the link in the Results pane, or switching to Manual mode.

Referenced Tuning Topics

What is Bandwidth

Excitation Type

Excitation Point

Excitation Current

FFT Settings

Torque Feed Forward

PL.KP - Position Loop Proportional Gain

VL.KI - Velocity Loop Integral Gain

VL.KP - Velocity Loop Proportional Gain6

VL.KI and PL.KP together

Low Pass Filter

Lead/Lag Filter

Post Processing Smoothing %