ASCII Objekt-Reference 

 

Home 

Screen page "PROFIBUS" 

The PROFIBUS-specific parameters, the bus status, and the data words in the transmit and receive directions, as seen by the bus-master are displayed on this screen page. This page is helpful when searching for errors and commissioning the bus communication. 



Baudrate 

The baud rate that is given by the PROFIBUS master is shown here.
 


PNO Identification 

The PNO identification is the number for servoamplifier in the list of ID-numbers of the PROFIBUS user organization.
 


Address 

Station address of the amplifier. The address is set up on the screen page �Basic setup�.
 


PPO Type 

The servoamplifier only supports PPO-type 2 of the PROFIDRIVE profile.
 


BUS status 

Shows the present status of the bus communication. Data can only be transferred across the PROFIBUS when the "Communication OK" message appears.
 


Input/Output-Buffer 

The data for input/output are only transferred, if the threshold monitoring for the servoamplifier has been activated in the master’s hardware configuration. 

Output 

The last bus object that was received by the master. 

Input 

The last bus object that was sent by the master.