ASCII Objekt-Reference 

 

Home 

Screen page "Encoder" 

Cycle time of the encoder emulation: 0.125 µs. 



Encoder emulation 

ASCII: ENCMODE 

Default: 1 

valid for all OPMODES 


Change this only while the amplifier is disabled.
 


Resolution ROD 

ASCII: ENCOUT 

Default: 1024 

valid for all OPMODES 

Determines the number of increments per turn that are output. Change this only while the amplifier is disabled. 

Encoder function (ENCMODE) 

Feedback system 

Resolution 

Zero position 

ROD (1) 

Resolver 

256...4096 

one per revolution
(only if A=B=1) 

Encoder 

256...524288
(28 ... 219) 

one per revolution
(only if A=B=1) 

ROD interpolation (3) 

Encoder 

22 … 27 (multiplication) TTL line x encoder resolution 

analog pass through from X1 to X5 

The resolution in the controls can be increased by quadruple evaluation of the increments. 



NI-Offset ROD 

ASCII: ENCZERO 

Default: 0 

valid for all OPMODES 

Determines the position of the zero (marker) pulse when A=B=1. The entry is referred to the zero-crossing of the feedback unit. 



Single / Multi Turn 

ASCII: SSIMODE 

Default: 0 

valid for all OPMODES 

Determines whether the output format is compatible to a single turn or multi turn SSI encoder. Change this only while the amplifier is disabled.
 


Baudrate SSI 

ASCII: SSIOUT 

Default: 0 

valid for all OPMODES 

Determines the serial transmission rate. Change this only while the amplifier is disabled.
 


SSI-Clock 

ASCII: SSIINV 

Default: 0 

valid for all OPMODES 

Determines whether the output level is normal, or inverted. Change this only while the amplifier is disabled.
 


SSI-Code 

ASCII: SSIGRAY 

Default: 0 

valid for all OPMODES 

Determines whether the output is in binary or GRAY code. Change this only while the amplifier is disabled.
 


ROD-Interpolation 

ASCII: ENCOUT 

Default: 16 

valid for all OPMODES 

Determines the multiplier for the number of lines of the feedback encoder per electrical motor rotation. 

Maximum output pulse number: 400,000 pulses/sec