ASCII Objekt-Reference 

 

Home 

Screen page "Motor" synchronous 

All the parameters that appear on this screen page are defined by the motor default values (internal database in the amplifier), and in most cases it will not be necessary to alter them.
 


Motor Type 

ASCII: MTYPE 

Default:1 

valid for all OPMODES 

This parameter is used to distinguish between synchronous (MTYPE = 1) and asynchronous motors (MTYPE = 3). If asynchronous is selected, then this screen page will appear in a different layout. Change this only while the amplifier is disabled.
 


No. of poles 

ASCII: MPOLES 

Default: 6 

valid for all OPMODES 

The current setpoint can be set for the operation of 2- to 250-pole motors. Change this only while the amplifier is disabled.
 


Io 

ASCII: MICONT 

Default: standstill current 

valid for all OPMODES 

The standstill current is the r.m.s. current value that the motor requires at standstill to produce the standstill torque (defines the maximum value for the entry of Irms in the current controller).
 


Iomax 

ASCII: MIPEAK 

Default: peak current 

valid for all OPMODES 

The peak current (r.m.s. value) should not exceed 4 x the rated current of the motor. The actual value is also determined by the peak current of the servo amplifier that is used (defines the maximum value for the entry of Ipeak in the current controller).
 


L 

ASCII: L 

Default: 0 mH 

valid for all OPMODES 

Inductance of the motor (phase-phase). You can take this value from the motor manual.
 


Max. speed 

ASCII: MSPEED 

Default: 3000 rpm 

valid for all OPMODES 

Maximum permissible speed of the motor. Limits the entry for the parameter SPEED LIMIT (screen page "Speed controller").
 


Number / Name 

ASCII: MNAME 

Default: blanks 

valid for all OPMODES 

ASCII: MNUMBER 

Default: 0 

valid for all OPMODES 

Select the motor that is used from the motor database. The data are loaded after the motor has been selected. If an encoder is used as a feedback unit, the motor number will automatically be reported to the servo amplifier. Make changes only while the amplifier is disabled. 

The following parameters are updated from the parameter set in the motor database: 

Screen page 

Parameter 

Basic Setup 

Max. Mains Voltage 

Motor 

No. Of Poles, Io, Iomax, L, Max.speed, Current Advance, Start Phi, Limit Phi, Brake with dialogue box 

Feedback 

Feedback Type, No. Of Resolver Poles, Offset 

Current controller 

KP, Tn 

Speed controller 

KP, Tn, PID-T2, Feedback, Max.speed, Overspeed 



Brake 

ASCII: MBRAKE 

Default: 0 

valid for all OPMODES 

If you want to operate a 24V holding brake in the motor directly from the servo amplifier, this parameter can be used to enable the brake function. 

In the diagram in the Product manual you can see the time/function relationship between the ENABLE signal, the speed setpoint, actual speed value, and the braking force. Change this only while the amplifier is disabled + reset.
 


Current advance 

ASCII: MTANGLP 

Default: 0 °electr. 

valid for all OPMODES 

A current-dependent phase advance, to make use of the reluctance torque for motors with magnets embedded in the rotor. 



Start/Limit Phi 

ASCII: MVANGLB 

Default: 2400 rpm 

valid for all OPMODES 

ASCII: MVANGLF 

Default: 20 °electr. 

valid for all OPMODES 

The inductive phase shift between the motor current and the motor voltage can be compensated at high speeds. With the given voltage conditions, a higher torque can be achieved at the speed limit. Alternatively, the achievable speed limit can be increased by up to 30%.
The phase shift is increased (depending on the motor speed) linearly from the Start Phi value up to the final value = Limit Phi. The optimum setting depends on the motor type and the speed limit.
 


Motor Unit 

ASCII: MUNIT 

Default: 0 

valid for all OPMODES 

Defines the entry for motor speed.
If 1/min (rpm) is used, the setting for velocity/speed will be applied for VUNIT.
 


Load Data from disk 

Load a motor-parameter file from a data medium (hard disk, diskette). The servo amplifier must be disabled to do this.