EXTENCODER.POSITION
Description
Gets the external encoder (EEO) position.
General Information
|
Type |
R/W |
|
Units |
1/(2^64) |
|
Range |
-2^63 to +2^63 -1 OR 0 to EXTENCODER.POSMODULO |
|
Default Value |
0 Counts |
|
Data Type |
Integer |
Variants Supported
This parameter is only supported on AKD BASIC drives.
Fieldbus Information
|
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
|---|---|---|---|---|---|
|
Modbus |
1080 |
Yes | 64 bit | Yes |
M_01-05-11-000 |