Torque Feed Forward

The torque-based feedforward terms on the drive model the physics of a motor and allow the drive to command the appropriate current, even before the encoder has time to send data back to the drive. Torque-based feedforward terms lower following error with virtually no stability penalty.

Acceleration Feed Forward
Compensates for mass of the load, higher load = higher acceleration feed forward.
Velocity Feed Forward
Compensates for viscous friction.
Friction Feed Forward
Compensates for static friction.

Feed-forward gives a motion controller “knowledge” about the system that is being controlled. This allows current to be commanded directly to the motor without any delays and provides more accurate motion without an increase in servo bandwidth.

Referenced Keywords
Parameter Description Drive Keyword

IL.FRICTION

Current Loop Friction Feed Forward

IL.FRICTION

IL.KACCFF

Current Loop Acceleration Feed Forward

IL.KACCFF

VL.KVFF

Velocity Loop Feed Forward

VL.KVFF