EGEAR.ON
Description
The command EGEAR.ON starts the electronic gearing procedure according to the selected electronic gearing mode:
| Mode | Description |
|---|---|
| 0 | Gearing Off |
| 1 | Gearing On |
Change this parameter only when the motor is not moving (MOVE.MOVING = 0). If you attempt to make a change while the motor is moving, an F826, "Cannot execute during a move" fault is produced.
General Information
|
Type |
Command |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
Start Version |
N/A |
Variants Supported
This parameter is only supported on AKD BASIC drives.
Fieldbus Information
|
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
|---|---|---|---|---|---|
|
Modbus |
1068 |
No | 8 bit | No |
M_01-05-11-000 |
Related Topics