VM.STATE
Description
VM.STATE contains the state of the Virtual Machine. The following numeric values correspond to the following states.
- Valid program is currently being executed.
- There is no valid program in the drive.
- Valid program exists, not running now, but ready to go.
- Valid program has terminated.
- Program encountered run-time error.
- Program is invalid (e.g. bad CRC).
General Information
|
Type |
R/O |
|
Units |
N/A |
|
Range |
0 to 5 |
|
Default Value |
None |
|
Data Type |
Integer |
|
Start Version |
M_01-00-00-000 |
Variants Supported
This parameter is only supported on AKD BASIC drives.