WHEN.DRVHANDWHEEL
Description
Records the value of DRV.HANDWHEEL when the when-condition is satisfied. The when-condition is checked once per 250 microseconds.
General Information
|
Type |
R/O |
|
Units |
1/4,294,967,296 rev |
|
Range |
0 to 4,294,967,295 rev |
|
Default Value |
0 rev |
|
Data Type |
Integer |
Variants Supported
This parameter is only supported on AKD BASIC drives.
Fieldbus Information
|
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
|---|---|---|---|---|---|
|
Modbus |
1170 |
No | 32 bit | No |
M_01-05-11-000 |
Related Topics