WHEN.DRVTIME

Description

Records the value of DRV.RUNTIME when the when-condition is satisfied. The when-condition is checked once per 250 microseconds.

General Information

Type

R/O

Units

Seconds

Range

0 - 2,147,483 (~24.8 days)

Default Value

N/A

Data Type

Integer

Variants Supported

This parameter is only supported on AKD BASIC drives.

Fieldbus Information

Fieldbus

Index/Subindex

Object Start Version

Modbus

1172

M_01-05-11-000

Related Topics

DRV.RUNTIME | When