DRV.SWENABLE
Description
The following commands disable or enable the drive:
- 0 (disables the drive)
- 1 (enables the drive)
Before power can flow to the motor, the following must all be true:
- Drive is not faulted.
- DRV.SWENABLE* input (J4-6) is connected to I/O RTN.
- DRV.SWENABLE Parameter is set to 1.
General Information
|
Type |
R/W Parameter |
|
Units |
none |
|
Range |
0 to 1 |
|
Default Value |
0 |
|
Data Type |
Integer |
Variants Supported
This parameter is only supported on AKD BASIC drives.
|
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
|---|---|---|---|---|---|
|
Modbus |
1056 |
No | 8 bit | No |
M_01-05-11-000 |
Related Topics