MOVE.INPOSLIMIT
Description
Specifies the tolerance of Position Error (PL.ERR) within which the MOVE.INPOSITION flag will be set to 1 (True). Set MOVE.INPOSLIMIT before using MOVE.INPOSITION.
-
-
MOVE parameters are only valid when DRV.OPMODE = 2 and DRV.CMDSOURCE = 5.
General Information
|
Type |
R/W |
|
Units |
16 bit counts |
|
Range |
0 to 140,737,488,355,328 |
|
Default Value |
0 |
|
Data Type |
Integer |
Variants Supported
This parameter is only supported on AKD BASIC drives.
Fieldbus Information
|
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
|---|---|---|---|---|---|
|
Modbus |
1114 |
Yes | 64 bit | Yes |
M_01-05-11-000 |
Related Topics