VM.AUTOSTART

Description

VM.AUTOSTART specifies whether or not the program in the AKD BASIC starts executing automatically when DC power is applied.

  • 0 = Program does not start automatically
  • 1 = Program starts automatically

Set VM.AUTOSTART to 0 or 1 in the terminal in WorkBench and execute an NVSave.

General Information

Type

R/W

Units

none

Range

0 to 1

Default Value

0

Data Type

Integer

Variants Supported

This parameter is only supported on AKD BASIC drives.

Fieldbus Information

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

1152

No 32 bit No

M_01-05-11-000