VM.RESTART

Description

Causes program execution to start again from the beginning of the program. Restart is the only way to exit from an Error Handler routine. Any interrupts, WHEN statements or loops in progress will be aborted.


  • VM.RESTART does not clear the user program variables or change any program variables, any predefined variables or have any effect on motor motion by itself .

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Variants Supported

This parameter is only supported on AKD BASIC drives.

Fieldbus Information

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

1154

No Command No

M_01-05-11-000

Related Topics

VM.START | VM.STOP