CAP0.EDGE, CAP1.EDGE
Description
The filtered trigger source is monitored for rising edge, falling edge, or both edges. The event mode logic may ignore the precondition edge detection; however, the trigger always uses edge detection.
The precondition logic has an identical feature controlled by CAP0.PREEDGE, CAP1.PREEDGE .
|
Value |
Description |
|---|---|
|
0 |
Reserved |
|
1 |
Rising edge |
|
2 |
Falling edge |
|
3 |
Both edges |
General Information
| Type |
NV Parameter |
| Units |
N/A |
| Range |
1 to 3 |
| Default Value |
1 |
| Data Type |
U8 |
| Start Version |
M_01-00-00-000 |
Variants Supported
| Variant | Supported |
|---|---|
| AKD Base | Yes |
| AKD with Position Indexer | Yes |
| AKD EtherCAT | Yes |
| AKD CANopen | Yes |
| AKD BASIC | Yes |
| AKD SynqNet | Yes* |
| AKD EtherNet/IP | Yes |
| AKD Profinet | Yes |
| AKD sercos® III | Yes |
| AKD-N | Yes |
| AKD-C | No |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Fieldbus Information
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
| Parameter |
Fieldbus |
Address |
Attributes | Signed? |
|---|---|---|---|---|
| CAP0.EDGE |
Profinet |
2027 |
Byte | No |
| sercos® III | 2 Octets | |||
| CAP1.EDGE |
Profinet |
2040 | Byte | |
| sercos® III | 2 Octets |
| Fieldbus | Parameter | Instance | Data Size | Data Type |
|---|---|---|---|---|
| EtherNet/IP | CAP0.EDGE | 28 | 1 Byte | Integer |
| CAP1.EDGE | 41 |
|
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
|
|---|---|---|---|---|---|---|
|
Modbus |
54 | CAP0.EDGE | No | 8 bit | No |
M_01-03-00-000 |
| 80 | CAP1.EDGE | |||||
Related Topics