CAP0.EVENT, CAP1.EVENT

Description

The event mode controls use of the precondition logic. If this field is not 0, then the precondition input is selected by CAPx.TRIGGER. If this field is 1, then the precondition edge is selected by the CAPx.PREEDGE. The four event modes are listed below.

Event

Description

0

Precondition settings ignored.

1

Trigger on first trigger event after selected edge on precondition input.

2

Trigger on first trigger event to occur while precondition input is 1

3

Trigger on first trigger event to occur while precondition input is 0.

Example

Event 0

The following diagram shows an example of Event = 0 (trigger on edge, trigger edge = rising). In this mode, the precondition logic is ignored.

Figure 1: Trigger Edge Mode

Events 2 and 3 (Trigger edge while precondition = 0 or 1)

In these events, the precondition logic samples the current (post-filter) state of the selected precondition source input. The capture engine looks for a trigger edge while the precondition input is at a “1” or “0” state.

Figure 2: Trigger edge WHILE precondition edge

 

Event 1 (Trigger edge after precondition)

In this event, each trigger event requires Enable=1, a new precondition edge, followed by a new trigger edge. The sequence requirements are shown in the figure below.

Figure 3: Trigger edge after precondition edge

Note: If the precondition and trigger edges occur at the same time, it is not a valid trigger event. A subsequent trigger edge must occur after the precondition edge. The same time resolves to a single 40 ns clock tick in the trigger event logic (after the optional filter function as well as any sensor, cable, or noise delays).

General Information

Type

NV Parameter

Units

N/A

Range

0 to 3

Default Value

0

Data Type

U8

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus Index/Subindex Object Start Version

EtherCAT COE and CANopen

3460h/5

CAP0.EVENT M_01-00-00-000

3460h/6

CAP1.EVENT
Paramter

Fieldbus

Address

Attributes Signed?
CAP0.EVENT

Profinet

2029

Byte No
sercos® III 2 Octets
CAP1.EVENT

Profinet

2042 Byte
sercos® III 2 Octets
Fieldbus Parameter Instance Data Size Data Type
EtherNet/IP CAP0.EVENT 30 1 Byte Integer
CAP1.EVENT 43
Fieldbus Index/Subindex Is 64 bit? Attributes Signed? Object Start Version
Modbus 58 CAP0.EVENT No 8 bit No M_01-03-00-000
84 CAP1.EVENT

Related Topics

Verwendung der Positionserfassung