CAP0.PREFILTER, CAP1.PREFILTER

Description

These parameters are not functional in M_01-03-00-000. In future releases, you can use DINx.FILTER to select a filter on the input channel.

General Information

Type

NV Parameter

Units

N/A

Range

0 to 2

Default Value

0

Data Type

U8

Start Version

End Version

M_01-00-00-000

M_01-03-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Parameter

Fieldbus

Address

Attributes Signed?
CAP0.PREFILTER

Profinet

2035 Byte No
sercos® III 2 Octets
CAP1.PREFILTER

Profinet

2048 Byte
sercos® III 2 Octets
Fieldbus Parameter Instance Data Size Data Type
EtherNet/IP CAP0.PREFILTER 36 1 Byte Integer
CAP1.PREFILTER 49

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

70

CAP0.PREFILTER

No 8 bit No

M_01-03-00-000

96

CAP1.PREFILTER

Related Topics

DIN1.FILTER TO DIN7.FILTER