CAP0.TRIGGER, CAP1.TRIGGER

Description

This parameter specifies the trigger source (capture input signal).

Trigger Source Input Name

0

General Input 1

1

General Input 2

2

General Input 3

3

General Input 4

4

General Input 5

5

General Input 6

6

General Input 7

7

X9 Connector, RS485 Input 1

8

X9 Connector, RS485 Input 2

9

X9 Connector, RS485 Input 3

10

Primary Index

11

Tertiary Index

General Information

Type

NV Parameter

Units

N/A

Range

0 to 11

Default Value

0

Data Type

U8

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus Index/Subindex Object Start Version

EtherCAT COE and CANopen

3460h/1

CAP0.TRIGGER

M_01-00-00-000

3460h/2

CAP1.TRIGGER

Paramter

Fieldbus

Address

Attributes Signed?
CAP0.TRIGGER

Profinet

2039 Byte No
sercos® III 2 Octets
CAP1.TRIGGER

Profinet

2052 Byte
sercos® III 2 Octets
Fieldbus Parameter Instance Data Size Data Type
EtherNet/IP CAP0.TRIGGER 40 1 Byte Integer
CAP1.TRIGGER 53

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

78

CAP0.TRIGGER

No 8 bit No

M_01-03-00-000

104

CAP1.TRIGGER

Related Topics

Verwendung der Positionserfassung

CAP0.PRESELECT, CAP1.PRESELECT