CMPx.ADVANCE

Description

Use this keyword to compensate for slow output devices such as relays or mechanical devices. The value of this parameter determines how long in advance the compare engine will trigger to compensate for a slow output.

For example, if CMP0.ADVANCE = 10, and CMPx.SETPOINT = 1,000,000 counts while the source is moving at 100,000 counts/sec (positive direction), then the compare will trigger when the source value crosses 999,000 counts. This will be 1000 counts early, or 0.01 seconds of 100,000 counts/sec.

CMPx.ADVANCE has a 0.001 ms resolution.

General Information

Type

NV Parameter

Units

ms

Range

0 to 30

Default Value

0

Data Type

U32

Start Version

M_01-13-00-000

Hardware Supported

Compare functionality is supported on hardware revisions D, DB, DA, and higher depending on the drive type. Check the label on the side of the drive to ensure the AKD meets one of the following requirements.

AKD Type Hardware Revision Supported
AKD Revision D or higher
AKD PDMM Revision DB or higher
AKD-T-IC Revision DA or higher

Variants Supported

Variant Supported
AKD Base No
AKD with Position Indexer No
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N No
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus Index/Subindex Object Start Version

EtherCAT COE and CANopen

53B1h /0

CMP0.ADVANCE

M_01-13-00-000
53B2h /0

CMP1.ADVANCE

Paramter

Fieldbus

Address

Attributes Signed?
CMP0.ADVANCE

Profinet

2945

DWord Yes
sercos® III 4 Octets
CMP1.ADVANCE

Profinet

2946 DWord
sercos® III 4 Octets
Fieldbus Parameter Instance Data Size Data Type
EtherNet/IP CMP0.ADVANCE 946 4 Byte Signed Float
CMP1.ADVANCE 947

Related Topics

Komparatoren (Vergleicher)