CMPx.ARM

Description

Use this keyword to arm or disarm a Compare setpoint. The setpoint value will only be compared against the Compare source (CMPx.SOURCE) if that setpoint is armed. If they match, an output pulse will be generated.

An error will be generated if CMPx.SOURCE, CMPx.MODBOUND1, CMPx.MODBOUND2, CMPx.WIDTH, and CMPx.MODEN are not set prior to enabling CMPx.ARM. If CMPx.SETPOINT is not set prior to enabling CMPx.ARM, the compare will trigger at the last set value, or the default value of 0 if the drive has been power cycled.

When accessing this keyword through a fieldbus, the values are to be interpreted as a bitmask, with each bit corresponding to one of the Compare setpoints.

Example

The following example arms setpoint 3 for CMP1.

-->CMP1.ARM 3 1

General Information

Type

NV Parameter

Units

N/A

Range

Argument 1: 0 to 7

Argument 2: 0 (Disarm) or 1 (Arm)

Default Value

0 (Disarm)

Data Type

Argument 1: Integer

Argument 2: Integer

Start Version

M_01-13-00-000

Hardware Supported

Compare functionality is supported on hardware revisions D, DB, DA, and higher depending on the drive type. Check the label on the side of the drive to ensure the AKD meets one of the following requirements.

AKD Type Hardware Revision Supported
AKD Revision D or higher
AKD PDMM Revision DB or higher
AKD-T-IC Revision DA or higher

Variants Supported

Variant Supported
AKD Base No
AKD with Position Indexer No
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N No
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus Index/Subindex Object Start Version

EtherCAT COE and CANopen

34C0h/1

CMP0.ARM

M_01-13-00-000
34C1h/1

CMP1.ARM

Paramter

Fieldbus

Address

Attributes Signed?
CMP0.ARM

Profinet

2914

Byte No
sercos® III 2 Octets
CMP1.ARM

Profinet

2915 Byte
sercos® III 2 Octets
Fieldbus Parameter Instance Data Size Data Type
EtherNet/IP CMP0.ARM 915 1 Byte Integer
CMP1.ARM 916

Fieldbus

Parameter

Index/Subindex

Is 64 bit? Attributes Signed?

Modbus

CMP0.ARM 1828 No 8 bit No
CMP1.ARM 1830

Related Topics

Komparatoren (Vergleicher)

CMPx.SETPOINT | CMPx.SOURCE