CMPx.OUTMASK
Description
This keyword sets the binary output disable mask between the setpoint and the drive's output pin. Note the internal setpoint state remains valid, only the external output is blocked.
Example
The following example sets an outmask to 7 (binary 111) to block setpoint states 0, 1, and 2 from asserting the drive output pin.
-->CMP0.OUTMASK 7
General Information
|
Type |
NV Parameter |
|
Units |
None |
|
Range |
0 to 255 |
|
Default Value |
0 (Inactive) |
|
Data Type |
Integer |
|
Start Version |
M_01-13-00-000 |
Hardware Supported
Compare functionality is supported on hardware revisions D, DB, DA, and higher depending on the drive type. Check the label on the side of the drive to ensure the AKD meets one of the following requirements.
| AKD Type | Hardware Revision Supported |
|---|---|
| AKD | Revision D or higher |
| AKD PDMM | Revision DB or higher |
| AKD-T-IC | Revision DA or higher |
Variants Supported
| Variant | Supported |
|---|---|
| AKD Base | No |
| AKD with Position Indexer | No |
| AKD EtherCAT | Yes |
| AKD CANopen | Yes |
| AKD BASIC | Yes |
| AKD SynqNet | Yes* |
| AKD EtherNet/IP | Yes |
| AKD Profinet | Yes |
| AKD sercos® III | Yes |
| AKD-N | No |
| AKD-C | No |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Fieldbus Information
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
| Fieldbus | Index/Subindex | Object Start Version | |
|---|---|---|---|
|
EtherCAT COE and CANopen |
5394h /0 |
CMP0.OUTMASK |
M_01-13-00-000 |
| 539Bh /0 |
CMP1.OUTMASK |
||
| Paramter |
Fieldbus |
Address |
Attributes | Signed? |
|---|---|---|---|---|
| CMP0.OUTMASK |
Profinet |
2916 | DWord | No |
| sercos® III | 4 Octets | |||
| CMP1.OUTMASK |
Profinet |
2923 | DWord | |
| sercos® III | 4 Octets |
| Fieldbus | Parameter | Instance | Data Size | Data Type |
|---|---|---|---|---|
| EtherNet/IP | CMP0.OUTMASK | 917 | 4 Byte | Integer |
| CMP1.OUTMASK | 924 |
Related Topics